LTspice

Fast • Free • Unlimited

LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation of analog circuits. Its graphical schematic capture interface allows you to probe schematics and produce simulation results, which can be explored further through the built-in waveform viewer.

Learn how to use LTspice with our tutorials below or dive deeper with our selection of helpful tips and articles. You can also browse our library of macromodels and demo circuits for select Analog Devices products.

Get to simulation faster with Tools to Generate LTspice Schematics below.

LTspice’s enhancements and models improve the simulation of analog circuits when compared to other SPICE solutions. Download LTspice below to see for yourself!

Download LTspice

Download our LTspice simulation software for the following operating systems:

Date models updated - Jul 8 2026

Download for Windows 10/11 x64 Version 26.0.2

Download for MacOS Version 26.0.2

Download for Windows 11 ARM64 Version 26.0.2

Download for Windows XP (End of Support)

Download for MacOS (17.2.4) (End of Support)

Download LTspice XVII for Windows (End of Support)

Get Support

Visit the LTspice Forum in EngineerZone to ask questions (or answer them) or add comments about LTspice.

LTspice EngineerZone Forum

Find Demo Circuits

Explore the entire library of ready-to-run LTspice demonstration circuits.

Explore demo circuits

Learn How to Use LTspice

Instructional Videos

A screenshot of LTspice software displaying a simple resistor-capacitor (RC) circuit simulation.
LTspice Basics

Learn the basics of using LTspice - creating a new schematic, running transient and AC simulations, and viewing results on the waveform viewer.

A screenshot of LTspice software displaying a behavioral circuit simulation.
Essentials Tutorial

Learn how to use transformers, add third party models, create, work with symbols, and more.

A screenshot of LTspice software displaying a phase shift circuit simulation.
AC & Noise Analysis Tutorial

Learn how to perform a basic AC analysis in LTspice as well as some capabilities you might not already know about. Also learn how to set up a noise simulation in LTspice to view both input and output referred voltage noise.

Title
Subtitle
Learn More

Tips and Articles

2d00 schematic of example circuit
Getting Started with LTspice

Learn how to use the most useful features in LTspice, whether starting with an example circuit, or drafting one from scratch.

Diagram of triangular and sawtooth waveforms in LTspice
Tips and In-Depth Articles

Our extensive collection of technical resources tackles a wide range of LTspice topics.

ltspice keyboard shortcuts
Keyboard Shortcuts

Keyboard shortcuts are an alternate way to invoke one or more commands in LTspice that would otherwise only be accessible by clicking through the menu or toolbar.

Title
Subtitle
Learn More

Tools to Generate LTspice Schematics

Get to simulation faster. These design tools export .asc files to create LTspice schematics.

Signal Chain Designer


Signal Chain Designer is a web-based platform for building and simulating sophisticated precision signal chains. It lets you evaluate your circuit’s behavior and examine transfer functions, noise performance, power consumption, input ranges, and DC errors. Experiment with different components and architectures and export your signal chain to LTspice to further verify your design.

Signal Chain Designer

Filter Wizard


The Analog Filter Wizard enables rapid design of low‑pass, high‑pass, and band‑pass active filters using real op‑amp models. Throughout the design flow, you can examine how the filter’s response transitions from ideal mathematical behavior to the performance dictated by actual device parameters and circuit‑level non‑idealities. The tool allows detailed evaluation of op‑amp trade‑offs—including gain‑bandwidth product, input‑referred noise, output swing limitations, and supply current—to identify components that meet your target specifications. When additional verification or transient analysis is required, the complete filter implementation can be exported directly to LTspice for further simulation.


Analog Filter Wizard



Analog Photodiode Wizard


The Photodiode Wizard provides a structured workflow for designing transimpedance amplifier (TIA) circuits for photodiode interfaces. You can select a photodiode from the built‑in device library or enter custom photodiode parameters such as junction capacitance, dark current, and responsivity. The tool enables rapid evaluation of key performance trade‑offs—including closed‑loop bandwidth, peaking (Q‑factor), and effective resolution metrics such as ENOB and SNR. Adjust TIA component values and immediately observe their impact through detailed plots of pulse response, frequency response, and noise‑gain characteristics. For comprehensive design validation, the complete TIA implementation can be exported directly to LTspice for further simulation and analysis.

Analog Photodiode Wizard

Precision ADC Driver Tool


The Precision ADC Driver Tool enables detailed simulation of precision ADC‑and‑driver signal chains. It identifies potential issues related to amplifier selection, input‑kickback settling, and distortion mechanisms, allowing rapid evaluation of architectural and component‑level trade‑offs. The tool computes and simulates key performance metrics—including system‑level noise, harmonic distortion, and time‑domain settling behavior at the ADC input—based on actual device parameters. When additional verification or transient analysis is required, the complete driver‑ADC configuration can be exported directly to LTspice for further simulation.

Precision ADC Driver Tool

LTpowerCAD


The LTpowerCAD® tool guides users throughout the supply design process, suggesting suitable parts to meet the user’s requirements according to the design’s power supply specifications. The tool shows real-time results of the feedback loop Bode plot, as well as the power stage performance, and can export the design to LTspice for full simulation and design verification.

LTpowerCAD

Related Resources
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project